Maintain synchronization of motor axes
Check out the case study of the SS1 (Safe Stop 1) function.
この動画の関連情報
あわせて見たい動画

Monitor speed of a motor running at limited speed
Check out the case study of the SLS (Safely-Limited Speed) function.

Turn off power to a specific process during changeover
Check out the case study of the SS2 (Safe Stop 2) function.

Monitor motor travel limits
Check out the case study of the SLP (Safely-Limited Position) function.

AC Servo System 1S Series with safety functionality: SS1 function
The SS1 (Safe Stop 1) function enables two axes to decelerate to a stop in a controlled manner while being synchronized during interlocking.

How to set up SS1 function in Automation Software Sysmac Studio
This video shows how to configure the SS1 (Safe Stop 1) function.

各モータ駆動部の同期ズレを回避
安全機能 SS1 : Safe Stop1の使用例をご紹介します。