Monitor speed of a motor running at limited speed
Check out the case study of the SLS (Safely-Limited Speed) function.
この動画の関連情報
あわせて見たい動画

Monitor motor travel limits
Check out the case study of the SLP (Safely-Limited Position) function.

Maintain synchronization of motor axes
Check out the case study of the SS1 (Safe Stop 1) function.

Turn off power to a specific process during changeover
Check out the case study of the SS2 (Safe Stop 2) function.

低速運転中のモータ速度を監視
安全機能SLS:Safely-Limited Speedの使用例をご紹介します。

AC Servo System 1S Series with safety functionality: SLS function
The SLS (Safely-Limited Speed) function monitors that a specified maximum motor speed is not exceeded when the protective cover is opened.

How to set up SLS function in Automation Software Sysmac Studio
This video shows how to configure the SLS (Safely-Limited Speed) function.