Monitor motor travel limits
Check out the case study of the SLP (Safely-Limited Position) function.
この動画の関連情報
あわせて見たい動画

Monitor speed of a motor running at limited speed
Check out the case study of the SLS (Safely-Limited Speed) function.

Maintain synchronization of motor axes
Check out the case study of the SS1 (Safe Stop 1) function.

モータ可動範囲の制限を監視
安全機能SLP:Safely-Limited Positionの使用例をご紹介します。

Turn off power to a specific process during changeover
Check out the case study of the SS2 (Safe Stop 2) function.

AC Servo System 1S Series with safety functionality: SLP function
The SLP (Safely-Limited Position) function monitors that the moving part is inside safe limits when the protective cover is opened.

How to set up SLP function in Automation Software Sysmac Studio
This video shows how to configure the SLP (Safely-Limited Position) function.