Turn off power to a specific process during changeover
Check out the case study of the SS2 (Safe Stop 2) function.
この動画の関連情報
あわせて見たい動画

Maintain synchronization of motor axes
Check out the case study of the SS1 (Safe Stop 1) function.

Monitor speed of a motor running at limited speed
Check out the case study of the SLS (Safely-Limited Speed) function.

品種替え時は対象工程のみ通電停止
安全機能SS2:Safe Stop 2の使用例をご紹介します。

Monitor motor travel limits
Check out the case study of the SLP (Safely-Limited Position) function.

How to set up SS2 function in Automation Software Sysmac Studio
This video shows how to configure the SS2 (Safe Stop 2) function.

AC Servo System 1S Series with safety functionality: SS2 function
The SS2 (Safe Stop 2) function enables two axes to decelerate to a stop with servo ON in a controlled manner while being synchronized, without cutting...