Object teaching
"E3AS-HF" Short distance detection including the workpiece with a single button press.
この動画の関連情報
あわせて見たい動画

Window object teaching
"E3AS-HF" Detect a workpiece (a mirror surface, irregular surface, or low reflectivity) that cannot be stably detected by object teaching.

Background reference teaching
"E3AS-HF" Detect a workpiece (a mirror surface, irregular surface, or low reflectivity) that cannot be stably detected by object teaching.

Detecting a workpiece passing on a roller conveyor with the spot beam type sensor
"E3AS-HF" Can stably detect only workpieces when it is installed so that the optical axis passes through the gap between the roller conveyors.

ワークティーチング
【E3AS-HF】1回のボタン押下で、ワークを含む近距離を検出

ティーチングの種類
【E3AS-HF】ティーチングの種類を紹介します。

背景基準ティーチング
【E3AS-HF】ワークティーチングで安定しないワーク(鏡面/凹凸がある/低反射ワーク)を検出