Detecting a small bore with the spot beam type
"E3AS-HF" Can detect a bore of 6 mm diameter (for vehicle model identification, etc.) by reducing the spot size.
この動画の関連情報
あわせて見たい動画

Detecting a workpiece passing on a roller conveyor with the spot beam type sensor
"E3AS-HF" Can stably detect only workpieces when it is installed so that the optical axis passes through the gap between the roller conveyors.

Sensing pallets with the diffuse beam type
"E3AS-HF" A lattice workpiece like a pallet can be stably detected by the sensor when the spot size is increased.

Angle characteristics of 85° max.
"E3AS-HF" Can stably detect a piece of black paper which a reflective photoelectric sensor cannot easily detect.

集光タイプによる小径穴検出
【E3AS-HF】スポットを小さくすることで車種判別用途などのΦ6mmの穴でも安定検知できます。

Detecting multicolor, low- reflective workpieces
"E3AS-HF" Can stably detect a transparent foldable container and a black-colored or chamfered cardboard box.

Detecting glossy black workpieces at a wide angle
"E3AS-HF" To detect an automotive body part at a 3-meter distance