Automatic Mutual Interference Prevention
"E3AS-HF" Can prevent interference between the sensors without the need for their channel settings.
この動画の関連情報
あわせて見たい動画

自動相互干渉防止機能
【E3AS-HF】チャネル設定不要で相互干渉を防止します。

Sensing pallets with the diffuse beam type
"E3AS-HF" A lattice workpiece like a pallet can be stably detected by the sensor when the spot size is increased.

Detecting a workpiece passing on a roller conveyor with the spot beam type sensor
"E3AS-HF" Can stably detect only workpieces when it is installed so that the optical axis passes through the gap between the roller conveyors.

Angle characteristics of 85° max.
"E3AS-HF" Can stably detect a piece of black paper which a reflective photoelectric sensor cannot easily detect.

シュリンク材の検出
【E3AS-HF】シュリンクされたペットボトルでも安定検出できます。

Detecting multicolor, low- reflective workpieces
"E3AS-HF" Can stably detect a transparent foldable container and a black-colored or chamfered cardboard box.