Sensing pallets with the diffuse beam type
"E3AS-HF" A lattice workpiece like a pallet can be stably detected by the sensor when the spot size is increased.
この動画の関連情報
あわせて見たい動画

Detecting a workpiece passing on a roller conveyor with the spot beam type sensor
"E3AS-HF" Can stably detect only workpieces when it is installed so that the optical axis passes through the gap between the roller conveyors.

Detecting a small bore with the spot beam type
"E3AS-HF" Can detect a bore of 6 mm diameter (for vehicle model identification, etc.) by reducing the spot size.

Angle characteristics of 85° max.
"E3AS-HF" Can stably detect a piece of black paper which a reflective photoelectric sensor cannot easily detect.

Sensing shrink wrappings
"E3AS-HF" Can stably detect a shrink-wrapped pack of plastic bottles.

Window object teaching
"E3AS-HF" Detect a workpiece (a mirror surface, irregular surface, or low reflectivity) that cannot be stably detected by object teaching.

Background reference teaching
"E3AS-HF" Detect a workpiece (a mirror surface, irregular surface, or low reflectivity) that cannot be stably detected by object teaching.