Codian Robotics社とのコラボレーションによるロボット統合ソリューション
オランダのロボットメカニクスの開発、製造会社であるCodian社が提供するロボットメカニクスとオムロンのコントローラのコラボレーション。統合コントロールによ...

オランダのロボットメカニクスの開発、製造会社であるCodian社が提供するロボットメカニクスとオムロンのコントローラのコラボレーション。統合コントロールによ...

We propose a new approach to control panel manufacturing incorporates environmentally considerations into the 'Value Design for Panel

Value Design for Panelに環境へ配慮した考え方を取り入れた新たな制御盤づくりを提案します。

半導体製造装置の付加価値向上に、NX-ECT101を用いたEtherCAT自律分散システムをご提案いたします。

ある・なし検出用途に必要な機能や性能を絞り込み、部材や製造工程を最適化。さらに新技術を駆使して驚きの価格を実現しました。大量にお使いいただくほどコスト...

【E3AS-HL】 複雑形状・色柄・光沢ワークの安定検出

【E3AS-HL】 反射板不要で柔軟な設計を実現

【E3AS-L】 単純形状・低反射ワークの安定検出

【E3AS-HL】 反射板不要で柔軟な設計を実現

【E3AS-HL】 複雑形状・色柄・光沢ワークの安定検出

"E3AS-HL" Flexible to design with no need for reflectors

"E3AS-HL" Reliable detection of complex-shaped, colored, patterned, or glossy workpieces

"E3AS-HL" Reliable detection of complex-shaped, colored, patterned, or glossy workpieces

"E3AS-L" Reliable detection of simple-shaped, low-reflective workpieces

"E3AS-HL" Flexible to design with no need for reflectors

【E3AS-F】 曲面・光沢・凹凸・多色ワークを安定検出

【E3AS-HL】 曲面・光沢・凹凸・多色ワークを安定検出

【E3AS-HL】 曲面・光沢・凹凸・多色ワークを安定検出

【E3AS-HL】 低反射曲面ワークを安定検出

【E3AS-F】 曲面・光沢・凹凸・多色ワークを安定検出

検出面への水滴やホコリの付着をエアーで除去

Air blow unit keeps sensing surface clean, reducing false detections

"E3AS-HL" Reliable detection of curved, glossy, irregular, or various colored surfaces

"E3AS-F" Reliable detection of curved, glossy, irregular, or various colored surfaces

"E3AS-HL" Reliable detection of curved low-reflective surfaces

"E3AS-HL" Reliable detection of curved, glossy, irregular, or various colored surfaces

"E3AS-F" Reliable detection of curved, glossy, irregular, or various colored surfaces

お客様のアプリケーションに必要とされる、速度、慣性、および再現性に関する、高度な機能を提供。 高速サイクルタイムで、広い動作範囲と繰り返し精度、従来に...

H7CCは、水がかかる場所でも安心してお使いいただけます。H7CCの防水/防塵構造をご紹介します。

This will introduce that H7CC can be used in environments exposed to water or water cleaning.

This will introduce a function to indicate a replacement time of H7CC and a tool to calculate the replacement time.

This will introduce new and improved design of H7CC for easier use by 6-digit up/down keys with LED mounted.

H7CCのわかりやすい操作、LED実装の6桁上下キーや見やすいデザインをご紹介します。

H7CCの交換時期をお知らせする機能と交換時期を算出する計算ツールをご紹介します。

ワークの形状、色柄や光沢などが変わる度に、センサの選定が必要で、装置を再設計することがありました。E3ASシリーズなら、複雑な形状、色柄、光沢の影響を受け...

E3ASシリーズなら、ティーチング方式で誰でも簡単に最適な設定ができ、立上げ時のトラブルによる後戻りをなくします。

量産稼働時に、現場の環境起因によるセンサの誤動作やセンサの破損でライン停止が発生し、復旧工数がかかることがありました。E3ASシリーズなら、検出面の保護で...

E3ASシリーズなら、文字が読みやすく分かりやすい有機ELディスプレイとティーチング方式で誰でも簡単に最適な設定ができます。

検出が難しいワーク(曲面、光沢、鋳物表面)に対し、設計・立上げ時の誤検出でセンサの再選定や設置調整が必要なことがありました。E3ASシリーズなら、曲面、光...

新規設計や設備改造のときに、センサの設置制約のために設備が複雑化し、設計工数がかかることがありました。E3ASシリーズなら、センサの設置可能な場所を拡大し...

難ワーク検出や長距離検出が必要な場合、回帰反射形のセンサを使用していましたが、装置の高度化、複雑化に伴い、設置スペースの制約があり、設計工数がかかって...

Sensor space limitations make equipment design and retrofit work complicated, resulting in time-consuming work. The E3AS Series can be installed in ch...

E3AS Sensors allow virtually anyone to set optimal settings on the easy-to-read OLED display using the teaching method.

Retro-reflective sensors are used to detect difficult workpieces or where long sensing distance is needed. Designing with retro-reflective sensors is...

E3AS Sensors allow virtually anyone to easily set optimal settings using the teaching method, eliminating rework due to problems during commissioning.

When difficult-to-detect workpieces (curved, glossy, or casting surfaces) cannot be detected correctly, sensors need to be reselected or adjusted. The...

Conventional sensors have to be selected each time the shape, color, pattern, or reflectivity of the workpiece changes, so the equipment sometimes nee...

When a sensor malfunction or breakage due to the environment causes a line stoppage during mass production, it can take a long time to restart. With t...

2台のAnyFeederとスカラロボットを組み合わせたシステム。デモでは3種+2種の5種類の異なる部品の整列を実行。提供可能なサンプルプログラムでは1台のAnyFeeder...

これまで複数台のセンサで行っていた判別検査を、1台でシンプルに解決できるスマートカメラF430-F/F420-Fシリーズの特長をご紹介します。

検出面へのほこりや油の付着、曇りを防止

The antifouling coating on the sensing surface, which is the industry's first, prevents dust and oil from sticking to the sensing surface, and keeps t...


作るモノの高機能化や薄型化に伴い、ワークには様々な材質や状態が混在し、従来の三角測距方式レーザ変位センサでは測定が難しくなっています。 白色共焦点方式...

曲面部の形状変化に追従しながらセンサの位置を自動制御し、複雑立体形状も高精度に測定します。

鏡面反射物体や透明物体の検出も可能。検出物体の色や材質の影響が少ない高ロバスト性の限定反射形センサを紹介します。

センサ、基板、コネクタが一体化。実装不要で小型化に貢献するフォト・マイクロセンサ コネクタシリーズを紹介します。

組立工数削減&省スペース化に貢献するフォト・マイクロセンサSMDシリーズを紹介します。

検出距離を従来比約2倍に高めた近接センサ E2E NEXTの動作デモをご覧いただけます。従来品との比較と交換時間を短縮できる「e-治具」をご紹介。

Safety Relay Unit G9SE - Slim design to save mounting space --------------------------------------------- Find solutions with Omron!Visit our global p...

スリム形状で取り付け工数を50%削減するG9SEの特長をご紹介。