本文

USB driver for ZUV-C40H downloads download

This USB driver is used to establish a connection between the ZUV-C40H and a PC.

Download File

Update May. 9, 2022
Version information Ver.11.1.0
Applicable user Users of ZUV-C40H Smart Curing System
Applicable model ZUV-C40H
File name and size usb_driver_for_zuv-c40h_for_windows10_en.zip (265KB) usb_driver_for_zuv-c40h_for_windows7_en.zip (6.8MB)

Installation Procedure [open]

  1. Turn ON your PC and start up Windows.
  2. Connect the controller to your PC using the USB cable.
  3. Open the Control Panel and then select Device Manager.
  4. Expand Other devices. Right-click Silicon Labs CP210x USB to UART Bridge and then click Update Driver Software.
  5. Click Browse my computer for driver software.
  6. Click Browse to select the downloaded folder and then click the Next Button.
  7. Click the Install Button.

System requirements

Compatible OS Windows7 32-bit, Windows10 64-bit
Communications port USB
Precautions
  • The exclusive USB driver must be installed only when the controller is connected to your PC for the first time. From the second connection onwards, the USB driver is automatically recognized and does not need to be re-installed.
  • To install the USB driver, log on as an Administrator or a user with system access rights.

Amazonギフト券が当たる!

サイトユーザーアンケートに
ご協力ください

2025/11/30(日)まで

詳しくはこちら