usrmerge (37) unstable; urgency=medium

  [ Johannes Schauer Marin Rodrigues ]
  * Use $DPKG_ROOT in usr-is-merged.postinst. (Closes: #1050755)

 -- Marco d'Itri <md@linux.it>  Tue, 29 Aug 2023 02:14:10 +0200

usrmerge (36) unstable; urgency=medium

  * Added code by Andreas Beckmann to clean up the biarch libraries
    directories when they are not needed. (Closes: #1038853)
  * Changed postinst to not run convert-etc-shells again on already
    converted systems and to run update-shells to make sure that the
    new shells.state file introduced in bookworm is up to date.
    (Closes: #1033167)
  * Improved the instructions to deal with a mounted /lib/modules/,
    which can also happen on some Xen-based systems. (Closes: 1034346)
  * Greatly improved the error messages when commands execution fails
    (see #1037362).
  * Added a versioned conflict with libc-bin, only relevant for the
    conversion script. (Closes: #1037362)
  * Added a versioned conflict with dhcpcd. (Closes: #1038832)
  * Added a versioned conflict with libparted1.8-10. (Closes: #1038832)
  * Added a versioned conflict with lustre-utils. (Closes: #1038832)

 -- Marco d'Itri <md@linux.it>  Sun, 27 Aug 2023 13:56:49 +0200

usrmerge (35) unstable; urgency=medium

  * Partially revert and further change the fix for #1024596, because it
    was incomplete and would fail when the directory containing the RTLD
    (e.g. /lib64) did not exist in /usr. (Closes: #1025926)

 -- Marco d'Itri <md@linux.it>  Mon, 12 Dec 2022 00:36:05 +0100

usrmerge (34) unstable; urgency=medium

  * Stopped creating the empty biarch directories, because glibc >= 2.35-4
    does that in preinst. (Closes: #1024596)
  * preinst: use mountpoint(1) to check if /usr is standalone instead
    if comparing st_dev, because this does not work with BTRFS subvolumes.
    (Closes: #1023816)
  * Updated the versioned conflict with kbd. (Closes: #1022936)
  * Made debian/copyright machine-readable. (Closes: #1025684)
  * Fixed a typo. (Closes: #1022790)

 -- Marco d'Itri <md@linux.it>  Sun, 11 Dec 2022 18:59:21 +0100

usrmerge (33) unstable; urgency=medium

  * Added a version number to the conflict with cruft. (See #941998.)
  * convert-usrmerge: stop if /lib/modules/ is a mount point, which is
    common on User Mode Linux. (Closes: #1021180)
  * Implemented only for Hurd systems a modified algorithm provided by
    Samuel Thibault. (Closes: #1020463)

 -- Marco d'Itri <md@linux.it>  Mon, 10 Oct 2022 23:52:46 +0200

usrmerge (32) unstable; urgency=medium

  * convert-usrmerge: fix handling the link X directory case.
    The case in which the source and destination are a symlink and a
    directory (or a directory and a symlink) actually was never handled.
    (Closes: #1020312)
  * Updated the versioned conflict with libpng12-0. (Closes: #1020549)
  * Relabel for SELinux the newly created directories and /etc/shells,
    courtesy of Christian Göttsche.

 -- Marco d'Itri <md@linux.it>  Thu, 29 Sep 2022 05:51:16 +0200

usrmerge (31) unstable; urgency=medium

  [ Luca Boccassi ]
  * usr-is-merged.preinst: run the check on upgrades too, because something
    may have un-merged the system since the last install. (See #926699.)

 -- Marco d'Itri <md@linux.it>  Mon, 19 Sep 2022 13:26:09 +0200

usrmerge (30+nmu2) unstable; urgency=medium

  [ Luca Boccassi ]
  * Non-maintainer upload.
  * overlayfs: attempt to move directory before bailing out (Closes:
    #1020228)

  [ Dimitri John Ledkov ]
  * Update regexp for new (temporary) ldd output

 -- Luca Boccassi <bluca@debian.org>  Sun, 18 Sep 2022 21:20:53 +0100

usrmerge (30+nmu1) unstable; urgency=medium

  * Non-maintainer upload.
  * maintainer scripts: shellcheck fixes
  * maintainer scripts: fix running arm64 on nspawn (Closes: #1019575)

 -- Luca Boccassi <bluca@debian.org>  Sat, 17 Sep 2022 02:12:55 +0100

usrmerge (30) unstable; urgency=medium

  * Use in usrmerge.postinst the same logic to determine if /usr is
    merged or not that was already being in usr-is-merged.preinst and
    convert-usrmerge. (Closes: #1019506)

 -- Marco d'Itri <md@linux.it>  Mon, 12 Sep 2022 01:10:54 +0200

usrmerge (29) unstable; urgency=medium

  * Made postinst skip convert-etc-shells too if the flag file is present,
    to avoid a piuparts failure.

 -- Marco d'Itri <md@linux.it>  Sun, 17 Jul 2022 18:12:29 +0200

usrmerge (28) unstable; urgency=medium

  * Reupload for the buildds.

 -- Marco d'Itri <md@linux.it>  Sun, 17 Jul 2022 11:12:03 +0200

usrmerge (27) unstable; urgency=medium

  * Created a dummy usr-is-merged package which will fail in preinst if
    the system does not have a merged /usr. (See the TC decision #994388.)
  * Implemented a flag file to skip the conversion, for the benefit of
    buildds. (Closes: #1008203)
  * Made postinst always fail if the conversion is not possible.
  * Made postinst fail if overlayfs is involved. (Closes: #1008202)
  * Removed the debconf question: now the conversion is unconditional.
  * Created a list of files in / to be ignored if also present in /usr, on
    request of Ubuntu. (Closes: #997866)
  * Conflict with cruft. (Closes: #1002888)

 -- Marco d'Itri <md@linux.it>  Thu, 14 Jul 2022 23:58:40 +0200

usrmerge (25) unstable; urgency=medium

  * Remove prerm, which has not been needed or even possibly used since
    usrmerge version 19 started removing /etc/dpkg/dpkg.cfg.d/usrmerge on
    upgrades. (Closes: #982867)
  * New debconf translation(s): es. (Closes: #987519)

 -- Marco d'Itri <md@linux.it>  Tue, 27 Apr 2021 01:21:48 +0200

usrmerge (24) unstable; urgency=medium

  * Moved the scripts to /usr/lib/usrmerge/ on request of Ubuntu for better
    FHS compliance.
  * README.Debian: removed a reference to /etc/dpkg/dpkg.cfg.d/usrmerge:
    the file can be ignored since it has been empty or missing since 2016.
    (Closes: #940077)

 -- Marco d'Itri <md@linux.it>  Sat, 16 Jan 2021 06:02:21 +0100

usrmerge (23) unstable; urgency=medium

  * Converted to dh.

 -- Marco d'Itri <md@linux.it>  Tue, 03 Sep 2019 02:20:46 +0200

usrmerge (22) unstable; urgency=medium

  * Added a version to the conflict with molly-guard (see #914716).
    (Closes: #914716)

 -- Marco d'Itri <md@linux.it>  Sun, 09 Jun 2019 14:54:21 +0200

usrmerge (21) unstable; urgency=medium

  * Added a version to the conflict with ebtables (see #912046).
  * Added a versioned conflict with arptables (see #916106).

 -- Marco d'Itri <md@linux.it>  Sun, 17 Feb 2019 17:44:25 +0100

usrmerge (20) unstable; urgency=medium

  * Use dh_perl to add a missing dependency on perl. (Closes: #915883)
  * Documented that packages can be removed while a conversion is in
    progress. (Closes: #914409)
  * Added a conflict with molly-guard, again (see #914716).
  * Added a conflict with ebtables (see #913883).

 -- Marco d'Itri <md@linux.it>  Sat, 08 Dec 2018 23:37:38 +0100

usrmerge (19) unstable; urgency=medium

  * Added a version to the conflict with safe-rm (see #759410).
  * Removed the /etc/dpkg/dpkg.cfg.d/usrmerge file which has been empty
    since version 11.

 -- Marco d'Itri <md@linux.it>  Sun, 30 Sep 2018 19:09:42 +0200

usrmerge (18) unstable; urgency=medium

  * New debconf translation(s): ru. (Closes: #883204)

 -- Marco d'Itri <md@linux.it>  Mon, 16 Jul 2018 03:58:40 +0200

usrmerge (17) unstable; urgency=medium

  * Defer the conversion of temporarily-broken symlinks in subdirectories
    too, to prevent leaving them broken if the program aborts.
    (Closes: #848504, #871706)
  * Added again a version to the conflict with molly-guard (see #837928).

 -- Marco d'Itri <md@linux.it>  Sun, 05 Nov 2017 19:14:38 +0100

usrmerge (16) unstable; urgency=medium

  * Added a version to the conflict with ksh (see #810158).

 -- Marco d'Itri <md@linux.it>  Wed, 31 May 2017 14:37:35 +0200

usrmerge (15) unstable; urgency=medium

  * Updated the version of the conflict with xfslibs-dev, because the
    package was broken again later (see #766811).
  * Added a version to the conflict with yp-tools (see #812532).

 -- Marco d'Itri <md@linux.it>  Tue, 21 Mar 2017 23:19:50 +0100

usrmerge (14) unstable; urgency=medium

  * Make convert-usrmerge restore the SELinux context for the newly
    created top level symlinks. (Closes: #850274)

 -- Marco d'Itri <md@linux.it>  Mon, 27 Feb 2017 02:03:26 +0100

usrmerge (13) unstable; urgency=medium

  * Do not run convert-usrmerge on NFS systems. (Closes: #842145)
  * Added a version to the conflict with elvis-tiny (see #813857).
  * Added a versioned conflict with libjson-c-dev (see #843145).

 -- Marco d'Itri <md@linux.it>  Mon, 12 Dec 2016 05:23:20 +0100

usrmerge (12) unstable; urgency=medium

  * Added a conflict with molly-guard. (Closes: #837925)
  * Updated the versioned conflict with zsh. (Closes: #824205)
  * New debconf translation(s): pt, de, nl, pt_BR.
    (Closes: #818636, 818656, 823443, 829342)

 -- Marco d'Itri <md@linux.it>  Thu, 29 Sep 2016 18:42:37 +0200

usrmerge (11) unstable; urgency=medium

  * dpkg.cfg: removed libpng12-0 (see #766809).
    No dpkg.cfg workarounds are used anymore.
  * After the conversion, use the new convert-etc-shells program to add
    to /etc/shells /usr-based paths for each shell in /. (Closes: #817119)
  * New debconf translation(s): fr. (Closes: #818144)

 -- Marco d'Itri <md@linux.it>  Tue, 15 Mar 2016 08:42:53 +0100

usrmerge (10) unstable; urgency=medium

  * dpkg.cfg: removed open-iscsi and tcsh (see #810276 and #767927).
  * Ask with debconf if convert-usrmerge should be run. (Closes: #797417)
  * New debconf translation(s): it.

 -- Marco d'Itri <md@linux.it>  Sun, 28 Feb 2016 02:02:03 +0100

usrmerge (9) unstable; urgency=medium

  * dpkg.cfg: removed acl, policycoreutils and musl-dev (see #767925,
    #767930 and #766812).
  * Added conflicts with elvis-tiny and yp-tools (see #813857 and #812532).
  * Added a version to the conflicts with mksh and zsh (see #807185 and
    #768079).
  * Updated the versioned conflict with davfs2, molly-guard and xfslibs-dev
    (see #812535 and #766811).

 -- Marco d'Itri <md@linux.it>  Wed, 10 Feb 2016 04:56:33 +0100

usrmerge (8) unstable; urgency=medium

  * Added Breaks with older cruft-ng and initramfs-tools.
    (Closes: #810860, #811317)
  * dpkg.cfg: removed coreutils.
  * Added a conflict with older open-vm-tools.

 -- Marco d'Itri <md@linux.it>  Fri, 22 Jan 2016 07:07:50 +0100

usrmerge (7) unstable; urgency=medium

  * On EBUSY, list the services using ProtectSystem.
  * dpkg.cfg: removed less and libbrlapi-dev.

 -- Marco d'Itri <md@linux.it>  Sat, 16 Jan 2016 03:51:37 +0100

usrmerge (6) unstable; urgency=high

  * Add support for ppc64el to directories_to_merge().
  * Check for free space in /usr before attempting the conversion.
  * dpkg.cfg: removed cryptsetup, libusb-0.1-4, xfsdump and xfslibs-dev.
  * dpkg.cfg: added open-iscsi.
  * Added a conflict with open-vm-tools.
  * Added a conflict with older vsearch.

 -- Marco d'Itri <md@linux.it>  Sat, 09 Jan 2016 04:33:13 +0100

usrmerge (5) unstable; urgency=medium

  * Create empty multilib and multiarch library directories.
    (Closes: #810091)
  * dpkg.cfg: removed davfs2, kbd and libdm0-dev.
  * Added a conflict with ksh.

 -- Marco d'Itri <md@linux.it>  Thu, 07 Jan 2016 02:55:40 +0100

usrmerge (4) unstable; urgency=medium

  * Fixed the conversion of symlinks with the same name in / and /usr,
    which was broken in many cases and broke libpng12-0. (Closes: #809495)
    The code still does not handle automatically all possible combinations,
    but we only need it to work around the few buggy packages with
    duplicated symlinks.
  * Preinst: check if an initramfs is being used.

 -- Marco d'Itri <md@linux.it>  Mon, 04 Jan 2016 05:12:46 +0100

usrmerge (3) unstable; urgency=medium

  * Added a conflict with mksh (see #807185).
  * debian/control: add the Homepage field. (Closes: #798056)

 -- Marco d'Itri <md@linux.it>  Sun, 27 Dec 2015 14:26:51 +0100

usrmerge (2) unstable; urgency=medium

  * Uploaded to the archive.

 -- Marco d'Itri <md@linux.it>  Wed, 05 Aug 2015 05:09:52 +0200

usrmerge (1) UNRELEASED; urgency=medium

  * Initial release.
  * Added a conflict with zsh (see #768079).

 -- Marco d'Itri <md@linux.it>  Tue, 04 Nov 2014 22:42:44 +0100